Personal and Professional Growth


Remanufacturing Associate

Mascot, TN, US, 37806


Your Career Begins at Timken
If you're ready for a challenging career that provides you with the ability to advance personally and professionally, look to Timken.  Our associates make the world more productive by improving the efficiency and reliability of the machinery that keeps industry in motion.

Job Title: Remanufacturing Associate

 

Description: Verify conformance of bearing components (cones) through visual and dimensional inspection using measurement instruments such as electronic bench gaging, dial indicators, and feeler gages.  Accept or reject parts according to industry and customer specifications.  Perform minor repairs including buffing, de-burring, and grinding using hand held rotary tools.  Maintain equipment and work stations through daily housekeeping and preventative maintenance activities. 

 

Overall Purpose: Inspect and repair bearing components (cones) in a safe manner, complaint with all requirements, while achieving delivery and productivity performance expectations.

 

Essential Functions: 

  1. Uses a master to set up the gauge block in order to properly measure the roller value.

     

  2. Determines the acceptability of roller sets based upon the values obtained.

     

  3. Scraps any non-conforming rollers that are found.

 

  1. Sets up closing press by changing dies based on order specifications.

     

  2. Aligns work piece against fixtures under ram as specified.

     

  3. Moves controls to lower ram that shapes parts or presses parts together.

     

  4. Fills cages with properly dimensioned/oriented tapered rollers.

 

  1. Places base cone into cone assemblies.

 

  1. Loads full cone assembly into closing press and operates press to close cage.

 

7.  Ensures that the application of a rust preventative is applied to the completed cone assembly.

 

  1. Operates an electric pallet jack.

     

  2. Aligns work piece against fixtures under ram as specified.

     

  3. May tend machine to separate parts or compress parts preparatory to assembly.

     

  4. Changes die heads to accommodate changes in bearing sizes.

 

  1. Changes the mandrel on the buffing wheel to the proper size for the inner race being buffed.

 

  1. Turns on the collection vent at the beginning of each shift and empties out any excess debris found within.

 

  1. Applies a flame retardant powder to the collection vent in order to prevent the debris particles from catching on fire.                     

     

  2. Ensures that materials are heated for the amount of time necessary for the annealing process to be completed.

     

  3. Removes all materials from the furnace after the annealing process in order to cool to room temperature.

     

  4. Visually inspects rollers under magnification, for conformance with AAR and customer specifications.

     

  5. Indicates acceptability of rollers through the use of a non-permanent marking pen.

 

Physical Demands & Frequency: Requires reaching, lifting, pushing/pulling, feeling and near acuity.

 

A.                Position: Standing/walking– 80%, bending – 20%.

 

B.                Weights & Force: Up to 50 plus pounds.

 

C.            Use of Controls: Operates cone press controls requiring both hands.

 

D.                Vision must be normal (20/20).  Correctional lenses are acceptable.

 

E.                Regularly required to reach with hands and arms, use hands to handle, manipulate or feel objects, tools, and/or controls

 

General Educational Development: Must have a high school diploma or GED equivalent. Information may be presented in written, oral or diagrammatic form and requires a common sense understanding to be applied in order to carry out the instructions.

 

Qualifications/Training: Must be able to understand and read decimals. Candidates shall successfully complete a training program and as applicable qualification requirements, as defined by the responsible functional manager. New hires shall demonstrate satisfactory performance during new hire probationary period

 

Training: On the job training provided.

 

Aptitudes:   Requires motor coordination, ambulatory capability, finger dexterity and manual dexterity.

 

Temperaments:  Able to perform repetitive or short-cycle work.

 

Environmental Conditions:   Frequent impact noise, seasonal heat.

                   

Protective Clothing and Personal Devices: Safety glasses, gloves and safety shoes.

 

All qualified applicants shall be treated equally according to their individual qualifications, abilities, experiences and other employment standards. There will be no discrimination due to gender or gender identity, race, religion, color, national origin, ancestry, age, disability, sexual orientation, veteran/military status or any other basis protected by applicable law.


 

 

 



The Timken Company designs a growing portfolio of engineered bearings and industrial motion products that improve the reliability and efficiency of global machinery and equipment to move the world forward. Timken posted $4.5 billion in sales in 2022 and employs more than 20,000 people globally, operating from 46 countries.
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
Nearest Major Market: Knoxville

Job Segment: Machinist, Inspector, Manufacturing, Quality